5G NR

PUCCH Test Configuration

Updated for 38.141 (v17.9.0 2023-5). Learn more.

Remote Command - PUCCH Test Config

User Interface - PUCCH Test Config

Remote Command - PUCCH Test Config

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:CONFig:PUCCh "PUCCHTestConfigType:F0T831|F1T8321|F1T8322|F2T8331|F2T8332|F3T834|F4T835|F1T83611|F1T83612|F0T837|F1T8381|F1T8382|F2T839|F3T8310|F0T8311|F1T83121|F1T83122|F3T8313,SubcarrierSpacing:SCS15K|SCS30K|SCS60K|SCS120K,Bandwidth:FR1BW5M|FR1BW10M|FR1BW20M|FR1BW40M|FR1BW100M|FR2BW50M|FR2BW100M|FR2BW200M,DuplexType:FDD|TDD,PhaseCompensation:AUTO|MANual|OFF,AdditionalDMRS:ON|OFF|1|0,NumberOfSymbols:<integer>,PUCCHFormat3Test:TEST1|TEST2,SlotConfigurationPeriod:MS0P5|MS0P625|MS1|MS2|MS1P25|MS2P5|MS5|MS10,NumberOfDownlinkSlots:<integer>,NumberOfDownlinkSymbols:<integer>,NumberOfUplinkSlots:<integer>,NumberOfUplinkSymbols:<integer>"

SCPI Example

RAD:NR5G:WAV:CCAR0:CONF:PUCC "PUCCHTestConfigType:F1T8321,SubcarrierSpacing:SCS30K,DuplexType:TDD,SlotConfigurationPeriod:MS5,NumberOfDownlinkSlots:5,NumberOfDownlinkSymbols:3,NumberOfUplinkSlots:4,NumberOfUplinkSymbols:1"

Couplings

PUCCH test configuration parameters and their default values are listed below:

PUCCHTestConfigType: F0T831,

Bandwidth: FR1BW100M,

SubcarrierSpacing: SCS30K,

DuplexType: FDD,

PhaseCompensation: AUTO ,

AdditionalDMRS: OFF,

PUCCHFormat3Test: TEST1,

NumberOfSymbols: 1,

SlotConfigurationPeriod: MS5,

NumberOfDownlinkSlots: 7,

NumberOfDownlinkSymbols: 6,

NumberofUplinkSlots: 2,

NumberOfUplinkSymbols: 4.

One combined string is needed to be inputted in SCPI command. The format of it is  "name: value , name: value …" .  Default value will be used if parameter is not provided.

The order of parameters does not matter. Parameter's name and value are case sensitive.

If parameter's type is enum and the inputted enum value is illegal ,  error " -224, Illegal parameter value; xxx has incorrect value." will be generated.

Initial S/W Revision

A.09.00, A.13.00

User Interface - PUCCH Test Config

GUI Location

Apps > 5G NR > Carrier UL > PUCCH Test Config

Initial S/W Revision

A.01.00

Modified S/W Revision

A.09.00, A.13.00

Couplings:

When PUCCH Test Config Type is ‘38.141-8.3.1 ACK missed detection for PUCCH format 0’, the ‘Number of symbols’ is visible to set.

When PUCCH Test Config Type is ‘38.141-8.3.4 UCI BLER performance for PUCCH format 3’, the ‘PUCCH Format3 Test’ is visible to select Test1 or Test2

When PUCCH Test Config Type is ‘38.141-8.3.4 UCI BLER performance for PUCCH format 3’ or ‘38.141-8.3.5 UCI BLER performance for PUCCH format 4’, the ‘Additional DMRS’ is visible to enable or disable additional DMRS. (For PUCCH Format 3 Test2, Additional DMRS is fixed to off).

Selects the PUCCH Test Config Type, the choices are defined in the section 8.3 of 38.141.

For ACK missed detection test, we use all ‘1’ as the payload.

For NACK to ACK detection test and UCI BLER test, we use PN9 as the payload.

Subcarrier Spacing

Bandwidth

Duplex Type

Phase Compensation

Number of Symbols

PUCCH Format3 Test

Additional DMRS

Subcarrier Spacing

Selects the Subcarrier Spacing.

Subcarrier

Spacing

(kHz)

FR#

Channel

Bandwidth

(MHz)

15

FR1

5

10

20

30

FR1

10

20

40

100

60

FR2

50

100

120

FR2

50

100

200

Bandwidth

Select the Bandwidth configuration for the carrier.

Subcarrier

Spacing

(kHz)

FR#

Channel

Bandwidth

(MHz)

15

FR1

5

10

20

30

FR1

10

20

40

100

60

FR2

50

100

120

FR2

50

100

200

Duplex Type

Choices: TDD | FDD

Selects the duplex type.

When TDD is selected, several TDD parameters appear below. These TDD parameters are reset to default values whenever numerology changes or FR changes. (The default values are different for each numerology.)

Transmission Periodicity

Sets the periodicity of DL-UL pattern. The choices are related to numerology.

Number of Downlink Slots

Sets the number of consecutive full DL slots at the beginning of each DL-UL pattern. The range is related to the numerology and slot configuration period.

Number of Downlink Symbols

Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP

Sets the number of consecutive DL symbols in the beginning of the slot following the last full DL slot.

Number of Uplink Slots

Sets the number of consecutive full UL slots at the end of each DL-UL pattern. The range is related to the numerology and slot configuration period.

Number of Uplink Symbols

Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP

Sets the number of consecutive UL symbols in the end of the slot preceding the first full UL slot.

Number of Special Slots

Displays the number of special slots.

TDD Slot Allocation

Displays the TDD slot allocation for one period.

Phase Compensation

Choices: Auto | Manual | Off

Default: Auto

Set the phase compensation mode on the baseband signal before upconversion.

Phase compensation is not applicable for PRACH carrier.

Auto: Use the RF frequency from the instrument node.

Manual: Enter the RF frequency manually.

Off: Disable phase compensation on baseband signal.

Number of Symbols

Choices: 1 | 2

Default: 1

Set the number of OFDM symbols when PUCCH Test Config Type is 38.141-8.3.1 ACK missed detection for PUCCH format 0.

PUCCH Format3 Test

Choices: Test1 | Test2

Default: Test1

Select the PUCCH Format3 Test when PUCCH Test Config Type is 38.141-8.3.4 UCI BLER performance for PUCCH format 3.

Additional DMRS

Choices: On | Off

Default: Off

Set additional DMRS for PUCCH format 3 and format 4.

PUCCH Test Config Update for 38.141 v17.9.0

Carrier Uplink